7/9/2009 10:23 AM | |
Posts: 272 Rating: (4) |
It seems that this happened on a already running system, please check the system configurator properties and see is it linked to your proj. |
7/10/2009 2:57 AM | |
Posts: 2661 Rating: (279)
|
Hi NimaMoaddeli, This behavior is because of the faceplates in the Water Library. I installed WL, tested and had the same problem! The solution is change the block name in CFC to MOTORand it'l work! This is only for W_MOT1, I haven't tested other blocks. This kind of block naming is probably Water Library naming convention, I haven't had time to read the manual. Looks like (the Water Library is) an interesting product... See attached screenshot. Regards AttachmentW_Mot1.pdf (209 Downloads) |
Last edited by: Phantom75 at: 7/10/2009 10:01 PMLast edited by: Phantom75 at: 7/10/2009 3:01 AM |
|
This contribution was helpful to1 thankful Users |
7/10/2009 9:24 AM | |
Posts: 272 Rating: (4) |
where do we use water lib?? |
Follow us on