7/1/2021 2:28 PM | |
Joined: 3/14/2008 Last visit: 5/14/2024 Posts: 2066 Rating: (928)
|
Hi, Yes, this is a familiar issue. A colleague has created a SR for this, but it will benefit us as user if you create a SR too. You can solve it by executing the following steps: 1. Open the OS project of each PC station (server/client) on the ES 2. In WinCC Explorer, go to Text Library and open the editor. 3. Right click: "Text Library" and select: "Remove Languages". 4. Delete Chinese language and save your settings. |
If I could help you, you can use the RATE button. Thank you. |
|
7/1/2021 3:04 PM | |
Joined: 3/14/2008 Last visit: 5/14/2024 Posts: 2066 Rating: (928)
|
Hi, No, UC01 has no problem (I used UC01 before without issue). It's because of the integration of Chinese language in the PCS7 media based on PCS7 V9.1. The UC02 has the same CFC and SFC update which is released for PCS7 V9.1. I'm working with UC02 for three months, haven't got any issue. You will if you reinstall UC02. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to2 thankful Users |
7/1/2021 4:29 PM | |
Joined: 2/29/2016 Last visit: 3/12/2024 Posts: 100 Rating: (1) |
Thnak you for the solution! I was dealing with the same problem, SR could not help me with the issue |