7/29/2022 9:45 AM | |
Joined: 8/3/2009 Last visit: 9/20/2024 Posts: 13753 Rating: (1732)
|
Hello yaramaz557 Yes we need more details of your program. perhaps you can make a few screenshots in we can see what is programmed on the object that is not working. Check also perhaps if there is only an inconsistency in the Runtime files: https://support.industry.siemens.com/cs/de/en/view/109778709 Bye Murof |
If this Information really helps, you could use the Rate function |
|
7/29/2022 1:39 PM | |
Joined: 12/6/2021 Last visit: 5/23/2023 Posts: 9 Rating: (0) |
Dear Murof When this Start-Stop button is active, the system starts and runs. When inactive, the system stops. In other words, it works and stops depending on a single input. There is no problem with software. Because I can see it running in PLCSIM. I matched the buttons as you can see in the attached photos. But it doesn't work. I do not understand. Do you have an idea? |
7/29/2022 1:40 PM | |
Joined: 12/6/2021 Last visit: 5/23/2023 Posts: 9 Rating: (0) |
|