4/9/2022 2:00 AM | |
Joined: 9/27/2006 Last visit: 12/4/2023 Posts: 12188 Rating:
|
Translation from the Portuguese text: From nute: "Good evening! I need toknow the specifications of the communication cable between a 6SL3210-1PC31-8ULO inverter (G120 PM240-2) and a PC. Olá nute; Os participantes do fórum da Siemens são de muitos países e muitos não entendem português. Para facilitar o entendimento entre os membros, escolhemos o inglês como idioma de intercâmbio. Por favor, tente escrever em inglês na sua próxima visita. Hello nute; Participants in the Siemens forum come from many countries, and many do not understand Portuguese. To make understanding easier between members we have chosen English as an interchange language. Please try to write in English on your next visit. The unit you are looking at is simply a power module for the control unit of the G120, and only a CU will communciate with Starter. What model of CU are you using? Look at the screenshot below, talen from the Siemens Industry Mall (electronic catalog), and verify your part number! The CU 230P-2PN for example will allow connection to your commissioning PC (Starter program) through standard USB cable or Profinet (standard Ethernet cable): https://support.industry.siemens.com/cs/ww/en/view/109782866/119456065035 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 04/11/2022 15:24:26Last edited by: The Helping Hand at: 04/12/2022 15:05:11Removed contact info |
|
This contribution was helpful to
1 thankful Users |
Follow us on