12/20/2013 8:23 AM | |
Posts: 461 Rating: (29) |
It is a tap.. The attached image s the one type of tank( For liquid gas ) I marked the area of water feeded ip... Regards, Nelliyan.G |
12/21/2013 6:07 AM | |
Joined: 9/16/2011 Last visit: 6/20/2024 Posts: 291 Rating: (6) |
I think it is not possible to use a proximity sensor, to detect the fully closed postion of the tap. is it ? otherwise, followMarcjanadvice.
|
Reg, |
|
12/28/2013 6:47 AM | |
Posts: 461 Rating: (29) |
Thanks all, some how i managed this by placing a photoelectric sensor by using a fixed test bed like a jig ,,,so that the operator cant move the tank once placed in test bed. So that if the thread wasnt threaded completely i will get a signal... this s working some how Perhaps i should have tried Marcjan idea before trying this .. Regards, Nelliyan.G |
Follow us on