5/26/2011 11:21 PM | |
Joined: 1/5/2007 Last visit: 4/7/2023 Posts: 1690 Rating:
|
Hi all, AttachmentCalculation_of_GAIN_and_OFFSET_for_analoge_amplifier_V3.zip (727 Downloads) |
Last edited by: O_Moderator at: 5/27/2011 7:21 AMsubject edited ==> Meine TAG-Listen: "deut." |
|
This contribution was helpful to
2 thankful Users |
4/23/2012 5:51 PM | |
Joined: 1/5/2007 Last visit: 4/7/2023 Posts: 1690 Rating:
|
Hello, with the LOGO! series 0BA6 and 0BA7 it is possible to calculate lineare functions (with block amplifiver) and polynoms as funtion of an analog value Ax (wilock Math. function). It is helpful to use MS-EXEL to calculate the coefficients of a polynome with oder 1 (linear) or up to 4 or 5. This coefficients are the basic to define the Parameters for a LOGO! circuit witch then can calculate a polynom (most as approximation for the real data). Her is the link to that tool: EXCEL tool polynom regression for linear and nonlinear calculations Best regards Betel |
==> Meine TAG-Listen: "deut." |
|
Follow us on