6/29/2021 1:50 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
hi GCosta, the value in the input-word is in 1/10° per unit. Have a look into the manual Selection tables for the SM 1231 RTD So you are checking if the temperatur is between 1°C and 2°C Do the values in IW150 and IW152 really come from HMI? regards, |
FCK WAR! |
|
This contribution was helpful to
1 thankful Users |
Follow us on