6/28/2013 1:32 PM | |
Joined: 3/14/2008 Last visit: 5/27/2024 Posts: 2069 Rating: (928) |
The licenses for PO are installed on the ES... You will have a total of 400 available. The PO will be "sent" to the CPU when downloading AS... Doesn't matter if you have more then one license.. |
If I could help you, you can use the RATE button. Thank you. |
|
6/28/2013 4:45 PM | |
Posts: 559 Rating: (87) |
Dear RKM, As you know PO means Process objects. Means How many Motors, PIDs or Valves Etc. you are going to use in your project, on the basis of that you calculate PO. so to calculate PO you must have P&ID for the process. Please go through the below link which will help you much better. How are the licenses for the AS and OS counted as from PCS 7 V7.0? |
6/28/2013 5:01 PM | |
Posts: 836 Rating: (100)
|
Hi, its totally woth checkin this FAQ to understand the basics... Actually it not up to date (the factor is 90, not 60)... |
6/29/2013 8:25 PM | |
Posts: 72 Rating: (6) |
Also u can go for the below link: |
6/29/2013 9:25 PM | |
Posts: 62 Rating: (4) |
Dear RKM, Pcs7 AS Licence is Depends on the how many Proce Objects are used in u Automation Station.Also How many Process Tags are required Will be displayed in the Project. For more details Please find Attached file. Regards, Avinashkrishna Bhimavarapu.
AttachmentPCS7 Licence Information.zip (456 Downloads) |
5/5/2014 10:01 AM | |
Posts: 340 Rating: (6) |
new question is splittet to I want to know the exact difference between AS PO and AS RT PO?. |