10/27/2022 8:35 AM | |
Joined: 6/29/2012 Last visit: 12/25/2023 Posts: 975 Rating:
|
Is there a possibility to check the used applicationmode (once or cyclic camming) of the Camin mode, after the axis is already synchronised. Off course you select the applicationmode yourself in the program, but to be completely sure when the axis is synchronised and the master still at standstill, you want to check everything before moving the master. You can see the f.i. the used master, but I see no feedback variable for applicationmode. |
10/28/2022 3:36 PM | |
Joined: 10/11/2006 Last visit: 3/13/2025 Posts: 5997 Rating:
|
Hello, you can only check" ApplicationMode" of the "MC_CamIn" command. |
With best regards, |
|