8/30/2019 10:37 AM | |
Posts: 5 Rating:
|
Hi, I've connected a direct-starter using Simocode Pro V PN, DM-F ProfiSafe digital module, current/voltage measuring module, earth module and operator panel. There is no PLC connected currently. I don't have a fault on my Simocode as the "Device" LED is green. On the DM-F ProfiSafe digital module, "Ready" LED is green and the "Device" LED is green. However, the "Out" LED is off and the "SF" LED is red. Can a DM-F ProfiSafe digital module be used without a F-CPU? Why is the "Out" LED off? How do you set the safety related output to be active? Why is the "SF" LED red? Is this because I haven't connected the DM-F ProfiSafe digital module to an F-CPU? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/30/2019 10:58:34New subject after splitting |
|
Follow us on