Industry Online Support
Technical Forum
4/18/2011 2:09 PM | |
Posts: 12 Rating:
|
[schnippschnapp] Can anybody tell me the maximum no. of SFC51 calls in one project for "CPU317 2 DP"? I guess the max. no of calls of SFC51 are limited to the type of CPU selected? Please comment Other questions were splitted to what's the difference between "SFC13" and SSL ID "B4" of "SFC51"?. problem while reading the diagnostic buffer of CPU 317 2DP by using SSL ID. issue related to "SFC51". |
Last edited by: O_Moderator at: 4/18/2011 2:50 PMnew subject after splitting |
|
4/18/2011 3:16 PM | |
Posts: 510 Rating:
|
The following link says that 4 concurrent SFC51 call is the maximum for an S7-300 PLC http://support.automation.siemens.com/WW/view/en/31977679 billwest |
3/11/2014 11:52 AM | |
Posts: 344 Rating:
|
new question is splittet to how much SFC51 can i call? (CPU 416-2 DP PLC). |
Follow us on