8/6/2012 1:05 PM | |
Posts: 22 Rating:
|
Hi there ))) I have the TP177micro panel 6AV6 640-0CA11-0AX1. The display isnt working normally, it doesnt show 90% of information. There`s a blue screen on it, but at the middle of a screen threre`s a band, part of screen that working normally (the photo`s are attached). So i think, that the HW and touchscreen of a panel is working great, the display is broken, cause when starting the panel, i can see the booting process, startup menu and mnemo in that 10 working percents of a screen. So. I want to backup the project from panel by WinCC 2008 Flex SP3. When i choose the backup command in wincc, i restart the panel, and then there is an error message, that saying to set the transfer mode in panel. Of course, i can`t, because i don`t see anything. I want to try do the backup BLINDLY. So, if anybody have same panel, can you send me video or pics with the instruction, where on screen i have to tap, step by step, to set the transfer mode on panel, and do the backup. It`s more likely that recreate the existing project Thank you for your help.
Attachmenttp177micro.zip (58 Downloads) |
Last edited by: Dan_Tien_Shan at: 8/6/2012 1:09 PM |
|
8/6/2012 1:13 PM | |
Joined: 4/22/2010 Last visit: 1/15/2025 Posts: 5697 Rating:
|
Hello, You can try How do you do an operating system update (OS update) on operator panels? Then you don't have to put the panel in transfermode. Regards, Marcjan |
Problem solved? |
|
8/6/2012 1:15 PM | |
Posts: 22 Rating:
|
ok. I`ll try. Thx a lot |
8/6/2012 2:16 PM | |
Posts: 3037 Rating:
|
Hello, How do you backup/restore with a Windows-based panel? You can find a picture from the loader and the transfer of TP177 micro in the following manual. See chapter 4.3.3 SIMATIC HMI HMI device OP 73micro, TP 177micro (WinCC flexible) Tweety |
Follow us on