9/15/2020 1:26 PM | |
Posts: 18 Rating:
|
As I understood if I add WISE-4010/LAN to my logo 8 I can get higher resolution for my analog input. In my case I want to connect 10 kg load cell and to read 10000 units. Will the LOGO read 10000 units (10000 grams in my case) from the load cell that is connected to the WISE-4010/LAN ? Also do I need additional Load Cell Amplifier or the load cell can go directly to the WISE-4010/LAN? Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/08/2020 13:17:56New subject after splitting |
|
Follow us on