11/27/2017 1:32 PM | |
Joined: 1/31/2017 Last visit: 9/27/2023 Posts: 1 Rating: (0) |
Hello, Can we connect 2 or more servo motor for example(v90) in paralell with one PLC pto comand, for example (PLC S7-1217 0+,0- , 1+,1- f outputs with[1, 2, 26 and 27] for 4 servo motors in one motion movment ) ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/29/2017 8:45:15 AMNew subject after splitting |
|
11/29/2017 11:48 AM | |
Posts: 103 Rating: (37) |
Best to use the pulse output of the one drive to feed into the next drive. Pulse outputs are listed on the right in the attached picture. |
Follow us on