2/9/2007 11:54 AM | |
Posts: 7 Rating: (0) |
Dear J_Bell, S5 side : IM308-C (Profibus DP master) PC side : CP5614 A2 (Profibus DP slave) I need an OPC server in order to use AIDMAP to see some variable progression in the S5 progam. I have Simatic net. I know the PC must be configured with NetPro (xdb file to import) but I don't know the link type to use. I tried S7 Link ans FDL link, but none worked. What must be the link configuration on the PC side ? Should a specific bloc be called in the PLC ? I join the project I created to configure the link. Please tell me what should I modify in order to make it work. Regards AttachmentS5.zip (836 Downloads) |
Follow us on