1/30/2020 1:14 PM | |
Joined: 9/9/2012 Last visit: 4/8/2025 Posts: 48 Rating:
|
Hello, Where to find the Simatic folder you say in Point2?? I have the same issue with a panel, in both machines that are twins: I mean that I download the same program to both machines; but it happens in only one machine,... I used version TIA PORTAL V15.1 updated 4 ---> I updated to V16 to see if it solves issue->NOT Another things that I have tried: Check that I am inside Siemens limits: PressHMI,Time stamp: 1/30/2020 11:42 AM - 3806736 bytes used of 12582912 bytes, maximum,0,13,11:41:06 AM
I only have 3 tags with continuous adquistion mode. I have reduced the most of the tags to refresh time 1 second. Checked internal script syntax OK No historical data no receipts No reports Also, What you can see in attached images. Any improvement? What it is strange is that it olny happens in only one machine of both identicals... ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/31/2020 08:40:25New subject after splitting There are 10 types of people in this world, those who understand binary and those who dont. |
|
Follow us on