Industry Online Support
Technical Forum
8/3/2007 11:30 AM | |
Posts: 9 Rating: (0) |
HI, CAN I CHANG THE NAME OF TAG WITHOUT DELETING THAT TAG? IF YES THEN HOW??? THANKS IN ADVANCE... NIRAJ CHANDRAKER |
8/8/2007 12:29 PM | |
Posts: 9 Rating: (0) |
hi, if the wincc version isv5.1 or 5.2then it is possible or not???? |
Last edited by: NIRAJ CHANDRAKER at: 08.08.2007 12:31 |
|
8/18/2007 1:53 PM | |
Posts: 9 Rating: (0) |
Dear Danielle , as u told it is not renaming..thanx for reply |
9/4/2007 12:53 PM | |
Posts: 5 Rating: (0) |
remember that u cannot rename tags while wincc runtime on. |
9/4/2007 1:34 PM | |
Posts: 1084 Rating: (72)
|
Except when the tag is just created not yet 'used'. You then even can delete it. ikkezelf |
9/7/2007 12:16 PM | |
Posts: 9 Rating: (0) |
it is not in the online condition...it is in the deactivate mode...i tried it but it is not possible.... Thanx to all of you.... |
9/10/2007 2:02 PM | |
Posts: 1275 Rating: (123)
|
Well... sorry then... As I said, I don't have v5 here, so I can't even try to find a workaround... sorry... Best regards, Danielle |
Follow us on