4/9/2017 6:28 PM | |
Joined: 3/28/2015 Last visit: 5/25/2024 Posts: 721 Rating: (213) |
Hello, 1-STEP 7 Professional / Basic V14 SP1 works together with WinCC, Startdrive, SIMOCODE ES and SOFT STARTER ESV14 SP1 and SIMOTION SCOUT TIA V5.1 in a single framework. STEP 7 Professional / Basic V14 SP1 (incl. WinCC Basic V14 SP1) can be installed on a PC in parallel with other versions of STEP 7 V11 to V13 SP2, STEP 7 V5.5 SP4, STEP 7 Micro/WIN V4.0 SP9, WinCC flexible 2008 SP3 and WinCC (from V7.2). 2-STEP 7 Professional / Basic V14 works together with WinCC, Startdrive and Scout TIA V14 in a single framework. STEP 7 Professional / Basic V14 (including WinCC Basic V14) can be installed on a PC in parallel with other versions of STEP 7 V11 up to V13 SP2, STEP 7 V5.5 SP4, STEP 7 Micro/WIN V4.0 SP9, WinCC flexible 2008 SP3 and WinCC (as of V7.2). |
Eng.Mohamed Ibrahim |
|