Industry Online Support
Technical Forum
9/12/2010 8:11 AM | |
Joined: 3/21/2006 Last visit: 12/18/2022 Posts: 10221 Rating:
|
Hello, Look at What should I do if I have set my PG/PC interface to ISO-Industrial Ethernet so I can use Routing with Starter and DriveES to access MICROMASTERS on Profibus from the network port on my PG or PC and I find that the communication doesn't work? plus How is a routing established from one PG via a PROFIBUS interface through a SIMATIC station to SINAMICS G120/G120D frequency inverter via a PROFINET interface? Best regards, Hristo Mihalev |
Follow us on