7/24/2017 2:03 PM | |
Joined: 1/19/2013 Last visit: 2/5/2023 Posts: 21 Rating:
|
WinCC TIA Portal Professional |
7/24/2017 4:25 PM | |
Joined: 8/3/2009 Last visit: 4/17/2025 Posts: 15311 Rating:
|
Hello kimich89 you can do it ether with screen windows: https://support.industry.siemens.com/cs/de/en/view/109339757 or with Faceplates: https://support.industry.siemens.com/cs/ww/en/view/68014632 I Think in WinCC Professional it wont be a problem to use a lot of these instances but It always depends on whtat you use in the different Screens. If its a small object with less functionality I would use a Faceplate. If its a bigger Object with more details and you have to use C Script or you have to get access to global information and so on then you have to use Screen Windows. Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
Follow us on