9/14/2023 9:22 PM | |
Joined: 5/12/2022 Last visit: 10/31/2023 Posts: 8 Rating:
|
Thank you so much! Creating a second DB did fix everything! I'll also move the the MC_Power to a separate network to keep it on whilst it makes sense. Just one more question, if I may: I have a simple PWM servo and I'm using a TO_SpeedAxis with the MC_MoveVelocity you just saw. But PWM servos are capable of absolute positioning. Can I use TO_PositionAxis with MC_MoveAbsolute with such simple case? I did try, but I get stuck when TIA asks me for an encoder that I don't have. All I want to do is to set a value between a range and set the PWM output to that value. I did try with manually writing to the write address, but people here in the forum recommended against it. Do you see a way out? Thanks!
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/15/2023 10:05:59New subject after splitting |
|
Follow us on