1/23/2019 6:28 PM | |
Joined: 10/14/2012 Last visit: 9/16/2022 Posts: 8 Rating: (0) |
Hello , In Tia V14 SP1 ,is there a problem ,if i install gsd Sinamics S120 CU320-2PN V4.7? I ask because i can not commnunicate with S120 and CPU 1515-3PN ,all is green and i have no any error. The all achses configuration in Scout V5.1 is completed ,i execute Script and install it in TIA V14 SP1,but i can not comunicate with CU,infeed and achses...Telegram and adreses is same in scout and Tia . Thanks in advance for your advice! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 1/24/2019 10:15:56 AMNew subject after splitting |
|
1/24/2019 7:18 AM | |
Joined: 10/14/2012 Last visit: 9/16/2022 Posts: 8 Rating: (0) |
Hello, sorry i want to say the topology is the same. The adresses is same in Tia Hardware and the programs block. |
1/24/2019 7:35 AM | |
Joined: 5/12/2006 Last visit: 6/4/2024 Posts: 22254 Rating: (2986)
|
Hello, Do you use Technology Objects with the drive or some FB to exchange the Data? Christoph |
1/24/2019 8:30 AM | |
Joined: 10/14/2012 Last visit: 9/16/2022 Posts: 8 Rating: (0) |
Hello, |
1/24/2019 8:32 AM | |
Joined: 10/14/2012 Last visit: 9/16/2022 Posts: 8 Rating: (0) |
Hello, HW TIA |
1/24/2019 8:36 AM | |
Joined: 10/14/2012 Last visit: 9/16/2022 Posts: 8 Rating: (0) |
Hello |