6/13/2018 7:02 PM | |
Posts: 1 Rating:
|
I have installed starter software V4.5 in windows 10, but could not connect the VFD using USB cable. In device manager I found the device with an yellow marking beside it. Need help to solve this issue. Product: Drive ES - Starter Release: V4.5.1.0 Copyright (C) Siemens AG, 1999 - 2016 Portions copyright 1991-2002 Compuware Corporation. Internal Identifier: 04.50.41.00 Internal Info: umc04.50.41.00release.1.vobadm Component: CrystalEdit Version: V1.0 Copyright (c) 1998-2008, Andrei Stcherbatchenko. All rights reserved. http://www.codeproject.com/KB/edit/crysedit.aspx ------------------------------------------------------------------------------------------ Product: DCC_EDITOR_SINAMICS Release: V2.4.1.0 Copyright (C) Siemens AG, 1999 - 2016 Internal Identifier: 04.50.41.00 Internal Info: umc04.50.41.00release.1.vobadm ------------------------------------------------------------------------------------------ Product: DCC_HELP_SYSTEM Release: V2.4.1.0 Copyright (C) Siemens AG, 1999 - 2016 Internal Identifier: 04.50.41.00 Internal Info: umc04.50.41.00release.1.vobadm ------------------------------------------------------------------------------------------ Component: SSP SIMOTION SINAMICS Int V4.8 Version: V04.80.21.00 Release: V04.80.65.00_02.10.60.00 Copyright (C) Siemens AG, 1999 - 2016 ------------------------------------------------------------------------------------------ Component: SSP SINAMICS DCP V1.2 Version: V01.20.01.00 Release: V01.20.08.00_19.81.00.00 Copyright (C) Siemens AG, 1999 - 2016 ------------------------------------------------------------------------------------------ Component: SSP SINAMICS HELP V4.8 Version: V04.80.21.00 Release: V04.80.65.00_02.10.60.00 Copyright (C) Siemens AG, 1999 - 2016 ------------------------------------------------------------------------------------------ Component: SSP SINAMICS V4.8 Version: V04.80.21.00 Release: V04.80.65.00_02.10.60.00 Copyright (C) Siemens AG, 1999 - 2016
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 6/25/2018 7:35:30 AMNew subject after splitting |
|
6/25/2018 1:52 PM | |
Joined: 10/11/2006 Last visit: 1/22/2025 Posts: 5985 Rating:
|
Hello, which drive you want to connect to? Basically our G120 drives comes with an USB interface. Please have a look at the following application example, where you can find a detailed explanation how to connect to you drive via USB and all necessary setting (PC/PC interface settings) https://support.industry.siemens.com/cs/de/de/view/60140921/en You software information doesn`t show any information about G120 SSPs. Please check that you have installed the corresponding STARTER to the used drive firmware and that the correct SSP is installed. You can find the G120 SSP here. https://support.industry.siemens.com/cs/de/de/view/109477753/en The latest G120 firmware https://support.industry.siemens.com/cs/de/de/view/109756820/en The latest STARTER version with a list of supported devices. https://support.industry.siemens.com/cs/de/de/view/26233208/en |
With best regards, |
|
Follow us on