10/12/2016 7:53 PM | |
Joined: 9/20/2012 Last visit: 2/2/2023 Posts: 17 Rating: (1) |
I have the problem that I saved the projects from the network to the local hard disk. When not connected to the network I can not open any project (also projects that are longer on the hard disk). Reconnected to the network projects on the hard disk will open. Traveld for nothing to customer, couldn't fix it. IT is also in the dark. Step 7 V5.5 Hotfix 11 Windows 7 Repair does not work because Temporary files are cleaned. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 10/13/2016 12:03:08 PMNew subject after splitting |
|
10/20/2017 3:09 PM | |
Joined: 4/12/2013 Last visit: 6/9/2022 Posts: 8 Rating: (2) |
Hello everyone, It looks like I have the same problem. When I am connected to the office network i can open my projects that are saved on the hard disk of my laptop. When my laptop is not connected to the network, i cannot open those same files anymore. Ater selecting project and click on OK, simatic mananger stays empty. In the lower right corner of simatic manager, selected: remains 0/0. I have version V5.6 + HF1 Revision level K5.6.0.1 Running on Windows 7 Professional (64-bit / service pack 1) No Rockwell software installed on laptop Update: I was connected to my network. Projects can be opened. I disconnect from network, and project can still be opened. Then restart laptop, without connecting to network. After that projects cannot be opened anymore. Then reconnect to network, projects can be opened. After disconnecting from network, project can still be opened. So it looks i have to be on the network while opening project once, after that it is irrelevant. |
Last edited by: Ruud@Leron at: 10/20/2017 3:32:18 PMLast edited by: Ruud@Leron at: 10/20/2017 3:34:09 PM |
|