10/28/2008 9:52 AM | |
Posts: 19 Rating: (0) |
Dear sir,
when i opened the project which was programed in S7 V5.4 in the pcs7 V6.1, it is popingup the error msg.I have attached the Screen Shot for the above error. Please let me know whether is it possible to install the saperate software S7 v5.4 by removing only the s7 v5.3 in my system which was already having pcs7 v6.1 without remove the pcs7. If Yes
VPK.... Attachmenterror HW.zip (209 Downloads) |
10/30/2008 11:22 AM | |
Posts: 19 Rating: (0) |
Thank You for your Kind Reply . VPK. |
10/30/2008 4:08 PM | |
Joined: 9/27/2007 Last visit: 12/18/2020 Posts: 993 Rating: (102)
|
Hello, you should notice that it is not recommendable to update only a part of PCS7. You better should think about updating the complete PCS7 to V7.x which includes Step7 V5.4 or program it again in PCS7 V6.1. Cumulus |
Learn more about visualization - visit the HMI courses of Siemens AG! |
|
Follow us on