12/16/2015 2:42 PM | |
Posts: 206 Rating:
|
Hell s_vb, the Siwarex CS is not made for bipolar applications. It is only able to measure 10% of the max. range as negative signal. The new modules WP321 (ET200SP), WP231 (S7-1200) are able to measure negative signals with full range. The Siwarex CF is also able to measure negative signals, but with much lower accuracy that the Siwarex CS. The Siwarex FTC (ET200M) is also able to measure negative signals with full range. For more information's about the modules look at http://siemens.com/weighing . Regards ABenno |
Follow us on