10/17/2022 6:29 AM | |
Joined: 7/5/2013 Last visit: 4/25/2025 Posts: 3149 Rating:
|
Hi Tim, Sm@rtClient is just exe-file and it should be possible to run it on Windows Server. What are the Sm@rtClient options for accessing a SIMATIC HMI Comfort Panel with control buttons using Sm@rtServer?: "... can be copied to any PC". Regards, Frink |
Pi is exactly three! |
|
This contribution was helpful to
3 thankful Users |
10/19/2022 11:26 AM | |
Joined: 8/3/2009 Last visit: 4/25/2025 Posts: 15355 Rating:
|
Hello T-V-R here you can also download the SmarClient separately: https://support.industry.siemens.com/cs/de/en/view/109482434 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on