8/31/2018 3:35 PM | |
Joined: 9/12/2013 Last visit: 7/4/2024 Posts: 32 Rating:
|
Hello, I have setup of S7-1500 PLC, IM 155-6 PN BA and Sinamics G120 drives as shown in attached file with all configuration and settings. Port X2 of PLC is connected to a switch which communicates with SCADA and if required we connect PG/PC for programming and Port X1 P1 R of PLC is connected to drives and Port X1 P2 R is connected to IM 155-6 PN BA. My problem is that I can connect the PG/PC to PLC via port X2 but I can't access drives from PG/PC from TIA portal V14 SP 1 project. Due to that I have to connect my PG to port X1 of PLC and then access drives. Can anyone suggest what I can do to fix this? Thank in advance. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 9/3/2018 10:08:55 AMNew subject after splitting |
|
9/3/2018 11:55 AM | |
Joined: 5/12/2006 Last visit: 3/14/2025 Posts: 22588 Rating:
|
for the drives, this devices you want connect or? |
Follow us on