4/7/2022 3:50 PM | |
Joined: 4/6/2021 Last visit: 2/4/2023 Posts: 4 Rating:
|
Hello, my name is Matheus and I have the same problem. Well, I have a router that is connected in corporate internet and my devices like PLC, controllers are connected in this router too in LAN connection. So, my structure is the internet arrives in WAN interface of router and my devices of process are connected in LAN interface. I control the PLC using WINCC application, but, using this configuration I can't to access the wincc application, the image with errors are attachment. But, when I connect my computer directly in the corporate internet I get to access the application. I need help to solve this problem ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/08/2022 08:56:39New subject after splitting |
|
Follow us on