3/6/2017 6:27 PM | |
Posts: 1 Rating:
|
Please ,I need your support! I have these modules: - PLC S7 200 (CPU 224-DC/DC/DC) -EM 277 (Profibus –DP) -CP 243-1(Ethernet) -KTP 600 DP Software: -Win CC TIA Portal V11 Basic -Step 7 MicroWIN V4.0 Cable Adapter: -Profibus(Simple Port and Programming Port) -MPI/DP(DB9-jack)----USB -PC/RS232(DB9-jack)---PPI/RS485(DB9-jack) -PPI(DB9-jack)—USB The positions of the DIP switches are 1-OFF,2-ON,3-ON,4-OFF. I can connect all the devices from PLC to PC, with one exception “PROFIBUS” (I want to mention that I have a Laptop and I don`t have any CP INTERFACE to ensure the connection between PLC and PC,through PROFIBUS). I can use separate the programs STEP 7 MicroWIN and WIN CC V11 Basic with my computer ,but I can not connect the HMI and PLC between them to my Laptop. The only connection which it`s working is : I am connecting the PLC to Laptop through CP 243-1 (TCP/IP(Auto)->Intel(R)ETHERNET)and in this way I have access to programming in STEP 7 Micro WIN and I connect the KTP 600 DP through PROFIBUS to EM 277 and I am using for that the Profibus programming port. Over the Profibus programming port I connect the MPI/DP---USB to my computer.In this way WIN CC V11 Basic it`s working,I can download also some programs,BUT I CAN NOT CONNECT THE HMI THROUGH PLC TO MY COMPUTER!!! In the connection of the Win CC did not appear S7 200!!! Thanks! ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 3/7/2017 2:54:18 PMNew subject after splitting |
|
Follow us on