12/4/2021 5:22 PM | |
Posts: 15 Rating:
|
I am only trying to activate the CIM at this time. The only purpose of the Logo!8 at this time is to verify that the Ethernet cable is OK, and the computer can communicate over it. I will link them after the CIM is working. I am not going through the router for the CiM connection. Router is for internet connection only. Wi-Fi is for connection to router. When Logo! 8 is connected to the ethernet cable Direct connect ethernet cable from PC to Logo! 8 using LogoSoft Logo Comfort shows: IP Address: 192.168.1.88 Subnet Mask: 255.255.255.0 Gateway: 192.168.1.1 MAC Address: E0-DC-A0-05-1E-20 Device Type: BM Status: Yes Will also connect to Logo! login page when IP is entered into browser When CIM is connected to the ethernet cable Direct connect ethernet cable from PC to Logo! 8 Using Windows 10 browser IP Address: 192.168.0.80 entered into browser https://192.168.0.80/ Also see the attached file showing Windows IP Configuration, Hope this is what you are looking for. Thanks, Dewey AttachmentCIM_IP.txt (485 Downloads) |
Follow us on