9/27/2007 11:35 PM | |
Joined: 9/26/2007 Last visit: 1/28/2024 Posts: 7 Rating: (0) |
Hello! At the beginning of the project all the information we got was this: - drawing of the hardware configuration - tag list - profibus configuration for CP342-5 The task was to create a visualisation for that system by connecting a PC with WinCC Flexible RT (we choose to use that program) and CP5611 to the CP342-5. As I understood from the information we had, since CP342-5 was defined as a slave, the PC with the CP 5611 should be the master. Later on, we got only the pictures of the HW config and config in NetPro. I think that ProTool you can see in NetPro is not used for the HMI, but only for downloading the program to the CPU. At first I thought that I set the wrong parameters in WinCC Flexible, but based on the information we have is it possible to make this connection? Thanks AttachmentWinCCflexible.zip (221 Downloads) |
9/28/2007 1:16 PM | |
Posts: 5822 Rating: (411) |
Hey Jesper... you are right! J_Bell |
3/5/2008 4:27 PM | |
Joined: 1/11/2007 Last visit: 10/31/2023 Posts: 8 Rating: (1) |
Gentlemen, 1,000,000 times "THANK YOU" for this discussion. Best Regard, Marino |
3/7/2008 5:09 PM | |
Joined: 9/1/2005 Last visit: 5/13/2024 Posts: 4100 Rating: (193) |
Hello Marino, thank you for that feedback! A Posting like yours is one of the reasons why I love our Technical Forum. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on