1/13/2015 12:09 PM | |
Joined: 9/9/2014 Last visit: 11/10/2021 Posts: 18 Rating:
|
Hi, For some reason the 1515-2 PN CPU is not showing up when I try to add it to my project tree. I only see 1511, 1513 and 1516 in the drop down menu. I installed all the latest support packages from here but that didn't help. Is there a GSD file somewhere i need to download? I am using TIA Portal V12 SP1. Thanks in advance |
1/13/2015 12:19 PM | |
Joined: 5/12/2006 Last visit: 3/18/2025 Posts: 22593 Rating:
|
Hi, you need TIA Portal V13.0 Update 3 to programm this PLC. show here Regards Christoph |
This contribution was helpful to
2 thankful Users |
1/13/2015 12:27 PM | |
Joined: 9/9/2014 Last visit: 11/10/2021 Posts: 18 Rating:
|
Damn. That's what I was afraid of. Well, I guess it's time to upgrade anyway. Thanks for the quick reply! |
Follow us on