1/28/2020 11:18 AM | |
Joined: 6/26/2017 Last visit: 9/27/2021 Posts: 7 Rating:
|
Hello.I have the following problem: I use TIA V15.1,some projects use 100% progam and HMI, other projects use Step7 Program and TIA only for HMI. when I want to upload the project to the HMI panel,I can't find the panel in the network.I use remote control via router,I can detect the PLC in the network,I can monitor the program Online, but I can't download anything on HMI (not detected). HMI is on the network because I can detect it with PING(see picture). I have this problem at all TIAs (V13, V14 and V15). thanks in advance!!! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/28/2020 13:55:54New subject after splitting |
|
Follow us on