10/12/2018 11:12 AM | |
Joined: 2/4/2015 Last visit: 12/28/2024 Posts: 67 Rating:
|
Dear all, We have G120 drive for drag chain conveyor application. Motor full load current is 14A. P0640 is set at 13A. We get overcurrent fault sometimes rarely. But we dont find the trend in Wincc for motor current to be more than 13A during fault. Why? Regards Surendhar M ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 10/12/2018 11:41:51 AMNew subject after splitting |
|
10/17/2018 11:36 AM | |
Joined: 2/4/2015 Last visit: 12/28/2024 Posts: 67 Rating:
|
Hi Sir, Then should i use r68[0]- Actual Current smoothed?? Regards Surendhar M |
Follow us on