11/3/2020 6:37 PM | |
Joined: 7/5/2013 Last visit: 4/24/2025 Posts: 3148 Rating:
|
Hello Sazu, you are using a TP1900 and compare it to a PC Runtime. On the PC you have drive C: but on the panel you don't. When you click the Downarrow-button in column Path, you see that you could store to storage card or, I guess, flash (\\). You have to store the data locally on the panel and then check the following FAQ for copying the data to a PC or NAS: Integrating HMI Operator Panels in TCP/IP Networks and access to a NAS or to a shared Windows folder Regards, Frink |
Pi is exactly three! |
|
This contribution was helpful to
1 thankful Users |
Follow us on