8/21/2014 8:58 AM | |
Posts: 1368 Rating:
|
Hello, Which connection type you use for connection to the PLC? Ethernet? MPI? If you use MPI, please check the parameters described here: http://support.automation.siemens.com/WW/view/de/10420976 |
8/21/2014 10:41 AM | |
Posts: 1368 Rating:
|
You said, after changing the MMC card, it works without errors. Do you try this mmc card (from the CPU 313) to another PLC? If it works, then if not, the mmc card seems to be defect. BTW: another post with the same error message /tf/WW/en/Posts/103940 please check also this... |
Last edited by: Pittiplatsch at: 8/21/2014 10:44 AM |
|
8/21/2014 11:40 AM | |
Joined: 2/11/2013 Last visit: 8/5/2023 Posts: 5 Rating:
|
PLC is functioning with that orignal MMC Card and the machine is in operation |
8/21/2014 1:21 PM | |
Joined: 2/11/2013 Last visit: 8/5/2023 Posts: 5 Rating:
|
I haven't tried orignal mmc with other 313. I will be in touch after testing that. Thanks for your help.
|
8/22/2014 8:09 AM | |
Posts: 1368 Rating:
|
Hey, have a look at this faq http://support.automation.siemens.com/WW/view/de/19215608 or http://support.automation.siemens.com/WW/view/de/26123822 can it be, that something like this is placed in your program? |
Last edited by: Pittiplatsch at: 8/22/2014 8:16 AM |
|
Follow us on