12/3/2020 10:23 AM | |
Joined: 2/10/2015 Last visit: 10/5/2024 Posts: 288 Rating: (1) |
Hello, thank you for the response. If I am following you when I opened STARTER, I clicked on search for training units. Online ... then, I created a project name then, I clicked on continue. then in access point I chose S7ONLINE and in PG / PC I chose my ethernet network card. Then I clicked on continue and the search for reachable subscribers started then some time later I saw the capture that I named 1 in the previous attached file and when I clicked on yes, some time later I saw the capture that I named 3 in the previous attached file. however, for the STARTER program it is in the same way that I proceeded and I was able to recover the program without concern. frankly I do not understand these instructions well: "In the screen i see no accessible nodes, only the starter project assist which should not be used. please try the accessible nodes in starter. is the G120 found in Simatic Manager if you use "Edit ethernet nodes"? " can you guide me maybe with examples on how to do it so i can solve my problem. you recommend me to try accessible nodes in starter and also you ask me if G120 found in Simatic Manager if you use "Edit ethernet nodes"? Here are some attached files of the hardware configuration of the PLC and the SIMOTION project. how should I modify the ethernet nodes and where (ie in STARTER or SIMATIC MANAGER). thank you for helping me
AttachmentHW.zip (318 Downloads) |
Last edited by: FRANCK HERVE at: 12/03/2020 10:24:41 |
|
12/4/2020 10:36 AM | |
Joined: 5/12/2006 Last visit: 10/8/2024 Posts: 22399 Rating: (3017)
|
you must enter exactly "NOTHING" only click on Parcourir and see what is found |
Follow us on