4/1/2018 11:22 PM | |
Joined: 12/29/2017 Last visit: 3/10/2022 Posts: 36 Rating:
|
Hello Christoph In my work I have to use a CPU 315-2 DP V3.3.11 with a Sinamic 6SL3040-0JA00-0AA0, it is of the S110 family, but I see that it is not included in stardrive Tia portal v13. I am installing on a V5 Starter virtual machine with all SSPs since it is not compatible with my native machine. My question is, can the environment of Starter V5 be worked with that of Step 7 v13 without problems? Or is that the case should I request another sinamics? I wait for your quick answer, thanks. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 4/3/2018 7:19:08 AMNew subject after splitting |
|
Follow us on