2/26/2018 9:39 PM | |
Joined: 1/5/2013 Last visit: 11/22/2024 Posts: 283 Rating:
|
Hello, Does SIEMENS support any new modules to be as DNP master in the S7-1200 or another CPUs or RTUs? I have power reclosers that support DNP 3, i'm searching for a good solution for that, I see that WinCC v7.4 with DNP driver can be DNP master, but my problem is that I have WinCC advanced V13 exists, so can the TCSB v3.0 with WinCC V13 can be a DNP master instead of WinCC v7.4? thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 2/27/2018 10:34:37 AMNew subject after splitting |
|
3/28/2018 1:19 PM | |
Posts: 118 Rating:
|
Hi, TCSB is a basic solution which supports the Siemens proprietary protocol "Telecontrol Basic". It doesn't support DNP3. |
Follow us on