11/23/2018 8:21 AM | |
Joined: 10/22/2018 Last visit: 6/6/2023 Posts: 9 Rating:
|
Can you help me. i have: - Module IM151-7F - PC adapter USB/MPI+ V2.0 - Profibus connector 6ES7972-0BB52-0AA0 can i use a PC adapter USB/MPI plug on connector 6ES7972-0BB52-0AA0 to upload programming to my PC? now position of switch on 6ES7972-0BB52-0AA0 is on (not off). ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/24/2018 9:26:12 PMNew subject after splitting |
|
11/23/2018 2:04 PM | |
Joined: 10/22/2018 Last visit: 6/6/2023 Posts: 9 Rating:
|
My module IM151-7F CPU (6ES7 151-7FA21-0AB0) has the programming in it. |
11/26/2018 10:08 AM | |
Joined: 8/3/2009 Last visit: 3/18/2025 Posts: 15016 Rating:
|
Hello in the manual of the IM151-7 CPU there is the Information that the RS485 Interface has external 24V (+/-) Pins. SO it should be forwarded through the Connector Plug and power the USB MP Adapter . Do you have tried already? does it Work?; i would say it should work. Sorry I cannot try we only use CP5711. Bye Murof |
Last edited by: Murof at: 11/26/2018 10:08:44 AMIf this Information really helps, you could use the Rate function |
|
Follow us on