3/2/2011 7:52 AM | |
Posts: 12 Rating: (0) |
Dear All, Can we implement CU310-PN with Sinamics S120 drives for tandom application (master-slave)? The master and slave drive has two different CU310-PN. Is it possible to communicate between two CU310-PN directly? If no,can twoCU320-2 DP's serve the purpose of sharing data? Please give your views on this. Regards Kul Splitted from homing and actual position with CU320 using MDI. |
Last edited by: O_Moderator at: 3/2/2011 10:05 AMnew subject after splitting |
|
Follow us on