2/28/2018 8:54 AM | |
Joined: 5/20/2015 Last visit: 5/29/2023 Posts: 209 Rating:
|
Dear all experts, i have 6ES7153-2AR04-0XA0 ET200M, IM153-2 INTERFACE REDUND.BUNDLE, it contains IM153-2 HF (6ES7153-2BA10-0XB0) AND Bus module for ET 200M for holding 2 IM153-2 red. (6ES7195-7HD10-0XA0). but in actual physical hardware integration IM153-2 HF is mounted on 6ES7195-7HB00-0XA0 (Bus module for ET 200M for holding two 40 mm wide I/O modules for removal and insertion function). will it works, i am getting bus fault on both bus BF1 and BF2. can we use6ES7195-7HB00-0XA0for connecting bothwhole rack of ET200M, IM153-2 INTERFACE REDUND.BUNDLE.with i/o modules help me ASAP. thank you. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 2/28/2018 1:49:26 PMNew subject after splitting Let's do it... |
|
2/28/2018 1:50 PM | |
Joined: 6/19/2017 Last visit: 5/26/2023 Posts: 6894 Rating:
|
|
My Forum is the place to personalize your profile, |
|
Follow us on