4/17/2008 9:32 PM | |
Joined: 4/6/2006 Last visit: 2/5/2024 Posts: 604 Rating:
|
Hi edec, With this information it is hard to give a proper diagnose on why the Station Configurator isn't starting. But to be honest I think this is a real compatibility issue. You mention that you use SIMTIC NET 6.2 SP1 combined with Win2003 SP1 this is not released for being used together. Which SIMATIC NET software component is enabled for which operating system? Without a Service Pack and if it's a R1 the software would be compatible but I think it's better to upgrade Simatic Net towards v2007. |
Best regards, |
|
4/17/2008 9:57 PM | |
Posts: 4 Rating:
|
The thing is that it has been running for the last few months with that same configuration. |
4/18/2008 5:54 PM | |
Joined: 4/6/2006 Last visit: 2/5/2024 Posts: 604 Rating:
|
Hello edec, thanks for your feedback. Yes it often has got to do with DCOM settings. It's kinda hard to handle. there are several FAQ's available on the CS Site about this topic. Commissioning PC Stations - Manual and Quick Start In chapter 18 is some information about DCOM. But since it's a Siemens document it's created with the Siemens software in mind. If you want a real DCOM Training the following institute is very interesting: http://www.opcti.com/ |
Best regards, |
|
7/5/2017 3:19 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating:
|
New question published by adnan.yousaf is split to a separate thread with the subject Cannot open the Station Configurator - Error "Verbindungsversuch fehlgeschlagen !". Best regards |
Follow us on