5/2/2012 3:49 PM | |
Joined: 4/19/2008 Last visit: 1/17/2023 Posts: 1525 Rating:
|
Can you tell me when you download Hardware are you able to See in the "Selecte Node Address" your PLC when you click on the View Button ? Which PLC you have & Which Protocol you used for the Communicating with PLC? What you have selected in the Set PG/PC interface ?
Can you tell me Have you installed the AS-OS Engineering ? Have a look on the FAQ & Select the AS-OS Engineering How do you install the WinCC Smart Tools? |
Ammy |
|
5/3/2012 12:00 PM | |
Joined: 4/24/2012 Last visit: 4/5/2023 Posts: 13 Rating:
|
Hi When I try to download the hole project I get the message. (See picture). This message comes beforeI get the "Selecte Node Address" window. If I try to download in hardware config nothing happens. I use interface protocol TCP/IP. This should be right since HW upload is working, online is working and also program change up/download is working. I also tried to make new project, with different cpu and without integrate WinCC project.But get the same problem. I use Step7 V5.5 SP2. (I just got this update.) BR Stefan AttachmentHWprob.zip (65 Downloads) |
Last edited by: Stefan_Norway at: 5/3/2012 12:14 PMI think my WinCC automatic TAG generating, (compile), is connected to the problem above. Since I cannot make downkload of hardware or netpro. Last edited by: Stefan_Norway at: 5/3/2012 12:00 PM |
|
5/3/2012 1:56 PM | |
Posts: 557 Rating:
|
hello, Check following: 1) verify local area connection IP & subnet 2) apply factory reset & reconfigure id again 3) try to upload default program. |
Follow us on