8/14/2023 2:10 AM | |
Joined: 8/29/2019 Last visit: 9/12/2024 Posts: 7 Rating:
|
Dear Sir, I'd like to ask about modbus TCP IP in Wincc Pro V17 (TIA V17). In Wincc 7, In modbus TCP IP driver I can choose CPU 984. In Wincc Pro, I can't find it. Could you help me? Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/14/2023 12:04:27New subject after splitting |
|
8/14/2023 2:30 PM | |
Joined: 5/30/2022 Last visit: 4/25/2025 Posts: 634 Rating:
|
Hi DUY BINH, WinCC Professional has some differences with classic WinCC, as you can see the equivalent of the WinCC Modbus TCP/IP driver is Modicon Modbus TCP/IP in which you only have to parameterize the network settings as you can see in the attached image, unless it is a Siemens equipment that you can use a specific Driver for Siemens equipment depending on the S7-300/400/1200/1500 range: Migration of connections (WinCC V7) What CPU/manufacturer are you trying to connect to? so I can help you to make the necessary parameterization. |
If this information really helps, you could use the Rate function. |
|
8/15/2023 10:14 AM | |
Joined: 6/25/2022 Last visit: 3/26/2025 Posts: 7 Rating:
|
Dear Sir, We use Wincc V7.3 modbus TCPIP direct connect to the DSLC-2 by Woodward with CPU type 984 and now we want to change to Wincc V17 but can not find it. Please help us Thanks |
Follow us on