5/19/2014 5:33 PM | |
Posts: 784 Rating: (52) |
Hello, Kindly explain this point? Best regards..... |
5/19/2014 5:58 PM | |
Posts: 784 Rating: (52) |
Hello, Is TIA V13 can open the projects programmed by TIA V12? Best regards...... |
5/19/2014 6:12 PM | |
Posts: 784 Rating: (52) |
Thankshuggy_d1 |
5/21/2014 5:20 PM | |
Posts: 18 Rating: (0) |
thank you Mr.huggy_d1 I Will try to install the following Packages: 1- Step 7 Professional V12 and then it's SP1 2- Step 7 Professional V12 UP3 or i need to install Updates from 1 to 3 ? 3- i have wincc V12 basic , should i install Wincc v12 basic Sp1 Too ?? Thank you Mahmoud |
5/21/2014 5:29 PM | |
Joined: 7/7/2010 Last visit: 9/20/2024 Posts: 15213 Rating: (2417)
|
Update 3 includes the updates for 1/2 so you can go V12, SP1, then update 3. Sadly, you may also have to install hardware support packs if your hardware does not appear in the catalog. WinCC you should install WinCC from your pro V12 install package, and apply the same SP and updates as are available. For the WinCC, I am not as well versed in the multiple licensing options to support the wide range of HMI products. Check the FAQs and WinCC forums for specifics if your license does not also include WinCC pro. |
science guy |
|
This contribution was helpful to2 thankful Users |
Follow us on