Industry Online Support
Technical Forum
2/18/2009 3:57 PM | |
Posts: 8 Rating: (0) |
Hi, |
2/19/2009 2:35 PM | |
Joined: 10/22/2008 Last visit: 2/16/2021 Posts: 59 Rating: (8) |
Hi Hasmas, did you use the following description to deinstall the SP3 of XP? http://support.automation.siemens.com/WW/view/en/31694896 Did you get a message that the download has finished? If not try it again and wait for this message. If you do not get this message you do not have enough rights for downloading the project. Because in the end of the downloading process the ES will open the project to change the computername in the wincc project. (This computername should be in you PCS7 project the name of your ES and will be change in the end of downloading to the name of the target OS.) Furthermore you can try to copy a file over network from your ES to your OS and try to open it. Perhaps you can login on both computers with Administrator Login and check if Administrator is on both computers in the user group "Simatic HMI". Amno |
Follow us on