6/29/2020 3:18 PM | |
Posts: 29 Rating: (0) |
I can change the time on a weekly timer from the HMI but I cannot select the days from the HMI pushbuttons. I have used the same address for both the TIA and LOGO but do not get any input in the timer when I press the button on the HMI ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/30/2020 06:19:02New subject after splitting |
|
6/29/2020 3:22 PM | |
Joined: 12/18/2014 Last visit: 6/8/2024 Posts: 33164 Rating: (4097) |
Please upload your LOGO! program and your HMI project as zip file. |
6/30/2020 10:57 AM | |
Joined: 12/18/2014 Last visit: 6/8/2024 Posts: 33164 Rating: (4097) |
As I wrote above:
|
6/30/2020 1:10 PM | |
Posts: 29 Rating: (0) |
AttachmentSteam Valve control.zip (106 Downloads) |
6/30/2020 1:26 PM | |
Posts: 29 Rating: (0) |
AttachmentSteam Valve Screen.zip (105 Downloads) |
6/30/2020 1:34 PM | |
Posts: 29 Rating: (0) |
Please note I have afactory to run so a little patience would be nice |
6/30/2020 1:59 PM | |
Posts: 29 Rating: (0) |
AttachmentSteam Valve Screen.zip (69 Downloads) |
6/30/2020 2:03 PM | |
Joined: 12/18/2014 Last visit: 6/8/2024 Posts: 33164 Rating: (4097) |
Again you only send the ap15.1 file alone. I give up.
|
6/30/2020 3:28 PM | |
Posts: 29 Rating: (0) |
try that one
AttachmentSteam Valve Screen.zip (63 Downloads) |
7/29/2020 11:19 AM | |
Joined: 12/18/2014 Last visit: 6/8/2024 Posts: 33164 Rating: (4097) |
Please upload your actually TIA project and the LSC program. |
7/29/2020 12:29 PM | |
Posts: 29 Rating: (0) |
please see below
AttachmentEnd Game.zip (51 Downloads) |
7/29/2020 12:34 PM | |
Posts: 29 Rating: (0) |
AttachmentEnd Game.zip (58 Downloads) |
7/29/2020 1:24 PM | |
Joined: 12/18/2014 Last visit: 6/8/2024 Posts: 33164 Rating: (4097) |
In both zip files are only the same lsc file. I need also the TIA projekt if you want help. |
7/29/2020 2:00 PM | |
Posts: 29 Rating: (0) |
please try this one
AttachmentEnd Game Screen.zip (47 Downloads) |
7/29/2020 6:34 PM | |
Joined: 12/18/2014 Last visit: 6/8/2024 Posts: 33164 Rating: (4097) |
Be glad that you have not given your project and LOGO! program to an official company for troubleshooting. It took me more than 3 hours to discover and correct all of your mistakes. And all mistakes because you didn't work properly. All errors that you could have found and fixed yourself. I won't do this again. The next time I just look in and if I find so many mistakes again, I won't do anything.
AttachmentEnd Game.zip (63 Downloads) |
7/30/2020 10:34 AM | |
Joined: 12/18/2014 Last visit: 6/8/2024 Posts: 33164 Rating: (4097) |
Did you activated the On/Off times of cam 2? |
7/30/2020 12:27 PM | |
Posts: 29 Rating: (0) |
yes that is on the timer itself I only activated the days required I will try and activate them all and see what happens. I |
7/30/2020 1:27 PM | |
Posts: 29 Rating: (0) |
ok thank you but I am still unsure what I did wrong? |