11/20/2020 12:00 PM | |
Joined: 6/28/2019 Last visit: 5/16/2024 Posts: 13 Rating: (5) |
Hi, I hope you can help me. I cannot simulate or even download the program into the HMI. I've done every step from the top post, ran WinCC Unified Configuration few times, created the project tree etc, but when I'm trying to go to the simulation mode I don't see the 'Load' window but Download to extend pops up showings 127.0.0.1 as IP address and no matter what i try it won't connect. Then when I try to download anything into HMI it doesnt work either. I've added the device in the network, made connection to plc etc but I cannot assign the device name - it comes with an error that device type is different and assign feature is not supported. When trying to go online (IP address is set in HMI and i can see it in accessible devices) it searches the hmi but highlights the IP address and doesnt allow to go online. I've been working with dozens Comfort Panels before and never had any issues with configuration or simulation... Any ideas what I am doing wrong or what's the best/easiest way to add HMI into project? Thanks for any help deborzanka ------------------------------------------------------------------------------------------ |
Last edited by: deborzanka1234567890 at: 11/20/2020 12:02:26Last edited by: Jen_Moderator at: 11/20/2020 13:11:33New subject after splitting |
|
11/20/2020 2:30 PM | |
Joined: 1/24/2017 Last visit: 1/25/2023 Posts: 12 Rating: (1) |
Make sure your settings in the control panel 'Transfer' settings are set to allow project download from the port you are using on the panel itself. Refer to the operator manual for the panels section 6.5 https://support.industry.siemens.com/cs/document/109773257 |
12/11/2020 10:49 AM | |
Joined: 6/28/2019 Last visit: 5/16/2024 Posts: 13 Rating: (5) |
Hi again, This is the error I'm getting when trying to start simulation: I'm really confused, do I need to set up a local IP address for the simulation? I watched few videos on YT about the simulation and there was no mention of IP address, it just worked straight away. For reference, I have S7-1200 PLC and MTP700 HMI, connected directly in the network PN/IE (not as the PC station and Scada RT as I don't have the license). PLC - HMI communications works ok, no issues. IP addresses: My HMI uses the access point S7ONLINE which has the following configuration in PC/PG interface: S7ONLINE (STEP 7) -> Realtek PCIe GBE Family Controller.TCPIP.Auto.1.<Active> I use these settings for ages, never had issues with standard Comfort Panel. Even when I download someone's project, the simulations doesn't work. I click on 'start simulation' and a get the following window: Has anyone had a similar problem or has an idea what is wrong in my setup? Attachmentfiles.zip (486 Downloads) |
Last edited by: deborzanka at: 12/11/2020 10:51:52Last edited by: deborzanka at: 12/11/2020 11:53:58Last edited by: Jen_Moderator at: 12/14/2020 14:20:09Removed link and added files as an attachment. |
|
Follow us on